How to assign interrupts for i.mx6ull in Config Tools for i.MX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to assign interrupts for i.mx6ull in Config Tools for i.MX

跳至解决方案
3,012 次查看
8Aineri
Contributor II

Good afternoon, dear NXP! How could I assign interrupts in this tool? I already configured all pins and now I have to assign interrupts for it and write my own interrupts handlers for all sorts of interrupts. But I cannot find how and where could I do this in this tool.

I am using Linux, so I think I somehow have to declare pin as a source for interrupt and then write driver to assign it to this pin but now I cannot understand how to do this.

P.S.

It is obvious to where I should put dtsi file, but where should I put another 4 (iomux_config.c(h), pin_mux.c(h)) generated files in SDK?

标签 (2)
0 项奖励
回复
1 解答
2,944 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @8Aineri 

I asked our Pin tool member, they said  the initialization of the interrupt vectors or interrupts from GPIO pins is not the part of the pins tool data for i.mx 6ULL.

The initialization of the GPIO interrupts are the part of the GPIO peripheral initialization and should be in the GPIO driver.

As the same thing that you mentioned.

B.R

在原帖中查看解决方案

4 回复数
2,945 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @8Aineri 

I asked our Pin tool member, they said  the initialization of the interrupt vectors or interrupts from GPIO pins is not the part of the pins tool data for i.mx 6ULL.

The initialization of the GPIO interrupts are the part of the GPIO peripheral initialization and should be in the GPIO driver.

As the same thing that you mentioned.

B.R

2,924 次查看
8Aineri
Contributor II

Thank you! I thought so, then, I'll do this in Linux style and all)

0 项奖励
回复
2,962 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi, @8Aineri 

As i know, The Pin tool from Config Tools seems don't have your request function(assign the interrupt for i.mx6ull), Also I will contact the owner double check this.

PS : I think this file are not used for put into SDK.Please see the attachment Chapter 3 for further understand.

 

2,961 次查看
8Aineri
Contributor II

I read this but I couldn't find a solution about how could I assign an interruption to pin. Maybe I should only mark pin as interruption and then write a linux driver manually but I couldn't find how to mark pin as interruption too.

How I could understand this - I cannot mark pin as interruption in this tool, I could only see is this pin could be an interruption or not and then I should do it in Linux Device Tree manually?

0 项奖励
回复