How to assign USB Audio as primary sound device in android4.4.2 system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to assign USB Audio as primary sound device in android4.4.2 system

3,567件の閲覧回数
mrleo
Contributor IV

Hi,all

My custom board is imx6q sabresd board,now I have two audio sound cards.

One is hdmi sound card,and another is usb audio sound card.

I known android 4.4.2 system is support usb audio.

Now I can found two sound cards in system.

I want to assign USB Audio as primary sound device in android 4.4.2 system.But not ok.

What should I do? Please,Anyone can give me some advices?

ラベル(3)
0 件の賞賛
返信
5 返答(返信)

2,265件の閲覧回数
saurabh206
Senior Contributor III

Hi

mrleo

There is different method to fulfill your requirement.

Simple solution is that you can disable HDMI sound from your kernel configuration.

In this case you will have only USB card registered.

Thanks

Saurabh

0 件の賞賛
返信

2,265件の閲覧回数
mrleo
Contributor IV

Hi,Saurabh Patel

First I use the Simple solution like you said,But in android 4.4.2 system open the record app,cannot record audio.and play audio also not hear sound.

I see logcat print some message like bellow.

W/audio_hw_primary( 2212): card -1, port 0 device 0x2

W/audio_hw_primary( 2212): rate 44100, channel 2 period_size 0xc0

E/audio_hw_primary( 2212): cannot open pcm_out driver 0: cannot open device '/dev/snd/pcmC4294967295D0p': No such file or directory

Thanks,

Leo

0 件の賞賛
返信

2,265件の閲覧回数
saurabh206
Senior Contributor III

Hi Leo,

Do you have USB device connected?

And usb audio enabled in your configuration?

0 件の賞賛
返信

2,265件の閲覧回数
mrleo
Contributor IV

Hi,Saurabh

Yes,USB device connected to the board.

about usb audio I can found in /proc/asound/cards.

cat /proc/asound/cards                                                        

card0/  cards                                                

0 [Device         ]: USB-Audio - USB Advanced Audio Device

                      C-Media Electronics Inc. USB Advanced Audio Device at usb-fsl-ehci.1-1.3, full

0 件の賞賛
返信

2,265件の閲覧回数
yixuan_guo
Contributor I

I think,

First of all ,Ignore other effects,you can use tinyplay to play a music to check the driver.

http://boundarydevices.com/hdmi/

0 件の賞賛
返信