Hi, all.
I'm using I.MX28 processor and now i try to make bootloader.
What i understood that sb file has bootloader information. I think, sb file has address where bootloader is stored.
But i couldn't find information about this.
What i want to know is that bootloader address where the data is stored. And, how to change this address.
In my system, first bootloader address is 0x100000 (512page), and second bootloader is 0xA80000(5376page).
I want to change second bootloader address to 0x20000(1024page).
Do you have any ideas?
解決済! 解決策の投稿を見る。
Hello,
One of i.MX28 features is using special (safe boot, .sb) format of executable images, which
is applied when USB recovery (boot) mode is used. Here we can apply corresponding
tools to convert .elf file to the .sb. Please refer to section 12.8 [Constructing Boot Image
(SB Files) to Be Loaded by ROM] of the i.MX28 Reference Manual.
Basically load addresses are provided by .elf file, so it is needed to rebuild .elf with
new linker options / file.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
One of i.MX28 features is using special (safe boot, .sb) format of executable images, which
is applied when USB recovery (boot) mode is used. Here we can apply corresponding
tools to convert .elf file to the .sb. Please refer to section 12.8 [Constructing Boot Image
(SB Files) to Be Loaded by ROM] of the i.MX28 Reference Manual.
Basically load addresses are provided by .elf file, so it is needed to rebuild .elf with
new linker options / file.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------