How to add support for NAND in IMX7 sabreSD board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add support for NAND in IMX7 sabreSD board?

3,500 Views
gopinathsriniva
Contributor III

Hello,

I have mounted NAND chip in IMX7 sabreSD board. Now I am trying to detect NAND in u-boot and kernel image. Also I want check NAND boot. In u-boot, I configured .config file from "mx7dsabresd_nand_defconfig and built the u-boot. But NAND boot is not working. It seems my NAND device is not detected in the u-boot. Output of nand device command is as below. 

=> nand device

no devices available

Is NAND support is already there in the u-boot code? Your ideas/suggestion will be much appreciated. 

Cheers,

Gopinath S

Labels (2)
Tags (1)
6 Replies

2,925 Views
mrshafie
Contributor II

hi. did you solve this problem? how to config for use nand ??? 

0 Kudos
Reply

2,940 Views
joanxie
NXP TechSupport
NXP TechSupport

what mx7 board you use? as I known, mx7 TO1.0 has issue for nand booting

0 Kudos
Reply

2,940 Views
jordan_chen
Contributor II

Hi Joan,

    I am a beginner for MCIMX7SABRE board and plan to boot from NAND flash too.

It seems like I have to modify following items to support NAND flash boot. Please kindly advice if any items I missed. Thanks.

 

Software:
1. Menu config for linux as below
(3.4.2.7 Menu Configuration Options of i.MX_Linux_Reference_Manual.pdf)
  CONFIG_MTD_NAND = y
  ...
  CONFIG_MTD_UBI = y
  ...

2. Do I have to set BOOT_FROM of imximage.cfg to nand?
(imx7-bsp-4.9.11-1/build-fb/tmp/work/imx7dsabresd-poky-linux-gnueabi/u-boot-imx/2017.03-r0/git/board/freescale/mx7dsabresd/imximage.cfg)

 

3. Do I have to modify DTS for NADN flash?

 

Regards,

Jordan

0 Kudos
Reply

2,940 Views
jordan_chen
Contributor II

Sorry, Add following item.

4. set UBOOT_CONFIG in local.conf to "nand" (i.MX_Yocto_Project_User's_Guide.pdf)

Regards,

Jordan

0 Kudos
Reply

2,940 Views
gopinathsriniva
Contributor III

Hi Joan,

I am using MCIMX7SABRE board. By default it has only NAND expansion. Not only NAND booting, I am also facing issues in detecting the NAND chip in u-boot. I enabled NAND driver by setting CONFIG_NAND_MXS=y in def_config file. Is that enough or I need to add few more support for detecting NAND ? 

0 Kudos
Reply

2,940 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check your imx7s part number on your board, if not TO1.0, then you need to configure the NAND in the uboot and kernel, for imx7s, we suggest you to use MT29F32G08CBADB,refer to the linux reference manual, 3.4.2.7 Menu Configuration Options
To enable the NAND driver, the following options must be set:
• CONFIG_IMX_HAVE_PLATFORM_GPMI_NAND= [Y]
• CONFIG_MTD_NAND_GPMI_NAND= [Y | M]
In addition, these MTD options must be enabled:
• CONFIG_MTD_NAND = [y | m]
• CONFIG_MTD = y
• CONFIG_MTD_PARTITIONS = y
• CONFIG_MTD_CHAR = y
• CONFIG_MTD_BLOCK = y
In addition, these UBI options must be enabled:
• CONFIG_MTD_UBI=y
• CONFIG_MTD_UBI_WL_THRESHOLD=4096
• CONFIG_MTD_UBI_BEB_RESERVE=1
• CONFIG_UBIFS_FS=y
Chapter 3 Storage
• CONFIG_UBIFS_FS_LZO=y
• CONFIG_UBIFS_FS_ZLIB=y