How to add ssi in TDM (network) mode to device tree imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to add ssi in TDM (network) mode to device tree imx6

跳至解决方案
3,424 次查看
j-g
Contributor III

Hello,

I'm currently trying to upgrade from kernel 3.0.35 to 3.10.17 and have been successful except for placing the ssi in network mode (8 channel TDM).  In kernel 3.0.35 I edited /sound/soc/imx/imx-sgtl5000.c to setup the ssi to SND_SOC_DAIFMT_DSP_A and SND_SOC_DAIFMT_IB_NF, also SSI_SCR_SYN and SSI_SCR_NET bits were being set (correct configuration for our hardware).  Can I accomplish this through the device tree?  If not what is the alternative?  I threw some printk statements in /sound/soc/fsl/imx-ssi.c but nothing printed out so I'm assuming the code is not being run, not sure.  Thanks for any help.

This is in my current dtsi file (which I'm assuming is setting I2S 2 channel mode, ssi is slave)

&ssi1 {

fsl,mode = "i2s-slave";
status = "okay";

};

标签 (6)
0 项奖励
回复
1 解答
2,616 次查看
fabio_estevam
NXP Employee
NXP Employee

With device tree the ssi driver is sound/soc/fsl/fsl_ssi.c.

sound/soc/fsl/imx-ssi.c only works with non-dt version.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,616 次查看
calebcrome
Contributor I

Hi there,

Have you had any luck getting TDM to work with the SSI port in Linux?  We're in need of that -- it would be super useful if you could share your experience, or even better, patches :-)

Thanks

-Caleb

0 项奖励
回复
2,616 次查看
jesseforgues
Contributor I

I am also interested in this topic.

0 项奖励
回复
2,617 次查看
fabio_estevam
NXP Employee
NXP Employee

With device tree the ssi driver is sound/soc/fsl/fsl_ssi.c.

sound/soc/fsl/imx-ssi.c only works with non-dt version.

0 项奖励
回复
2,616 次查看
j-g
Contributor III

Thank you very much Fabio for the information.  With that knowledge I'll be able to continue on for a bit.

0 项奖励
回复