Hi ALL,
We want to use sgtl5000 on sabresd_6dq. BSP is l5.0.0_1.0.0-ga. Now kernel is work ok, but play music error.
add file config_sgtl5000.h
modify hardware/imx/alsa/tinyalsa_hal.c
#define SUPPORT_CARD_NUM 8
/*"null_card" must be in the end of this array*/
struct audio_card *audio_card_list[SUPPORT_CARD_NUM] = {
&sgtl5000_card,
&wm8958_card,
&wm8962_card,
&hdmi_card,
&usbaudio_card,
&spdif_card,
&cs42888_card,
&null_card,
};
W/AudioTrack( 435): AUDIO_OUTPUT_FLAG_FAST denied by client
W/AudioTrack( 435): AUDIO_OUTPUT_FLAG_FAST denied by client
--------- beginning of system
I/ActivityManager( 435): START u0 {act=android.intent.action.PICK dat= typ=vnd.android.cursor.dir/track cmp=com.android.music/.TrackBrowserActivity (has extras)} from uid 10035 on display 0
V/PhoneStatusBar( 529): setLightsOn(true)
E/MetadataRetrieverClient( 170): failed to extract an album art
E/MetadataRetrieverClient( 170): failed to extract an album art
I/ActivityManager( 435): Displayed com.android.music/.TrackBrowserActivity: +147ms
W/AudioTrack( 435): AUDIO_OUTPUT_FLAG_FAST denied by client
E/MediaPlayer( 913): Should have subtitle controller already set
I/ActivityManager( 435): Start proc com.android.musicfx for broadcast com.android.musicfx/.ControlPanelReceiver: pid=1234 uid=10010 gids={50010, 9997, 3003, 3002} abi=armeabi-v7a
E/MetadataRetrieverClient( 170): failed to extract an album art
E/Zygote ( 1234): Zygote: error closing descriptor
E/Zygote ( 1234): android.system.ErrnoException: close failed: EBADF (Bad file number)
E/Zygote ( 1234): at libcore.io.Posix.close(Native Method)
E/Zygote ( 1234): at libcore.io.BlockGuardOs.close(BlockGuardOs.java:101)
E/Zygote ( 1234): at android.system.Os.close(Os.java:84)
E/Zygote ( 1234): at com.android.internal.os.ZygoteInit.closeServerSocket(ZygoteInit.java:204)
E/Zygote ( 1234): at com.android.internal.os.ZygoteConnection.handleChildProc(ZygoteConnection.java:880)
E/Zygote ( 1234): at com.android.internal.os.ZygoteConnection.runOnce(ZygoteConnection.java:267)
E/Zygote ( 1234): at com.android.internal.os.ZygoteInit.runSelectLoop(ZygoteInit.java:784)
E/Zygote ( 1234): at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:690)
E/MetadataRetrieverClient( 170): failed to extract an album art
I/MediaFocusControl( 435): AudioFocus requestAudioFocus() from android.media.AudioManager@1de47f28com.android.music.MediaPlaybackService$3@19f88441
V/MusicFXControlPanelReceiver( 1234): onReceive
V/MusicFXControlPanelReceiver( 1234): Action: android.media.action.OPEN_AUDIO_EFFECT_CONTROL_SESSION
V/MusicFXControlPanelReceiver( 1234): Package name: com.android.music
V/MusicFXControlPanelReceiver( 1234): Audio session: 9
V/MusicFXControlPanelEffect( 1234): openSession(android.app.ReceiverRestrictedContext@30db2a24, com.android.music, 9)
I/art ( 435): Explicit concurrent mark sweep GC freed 12808(682KB) AllocSpace objects, 2(32KB) LOS objects, 33% free, 6MB/9MB, paused 1.855ms total 85.434ms
D/NuPlayerDriver( 170): start(0x74e0d040)
I/GenericSource( 170): start
E/NuPlayer( 170): feedDecoderInputData getCurrentPosition failed.
E/NuPlayer( 170): feedDecoderInputData getCurrentPosition failed.
E/NuPlayer( 170): feedDecoderInputData getCurrentPosition failed.
E/NuPlayer( 170): feedDecoderInputData getCurrentPosition failed.
E/NuPlayer( 170): feedDecoderInputData getCurrentPosition failed.
E/NuPlayer( 170): feedDecoderInputData getCurrentPosition failed.
I/ActivityManager( 435): START u0 {act=com.android.music.PLAYBACK_VIEWER flg=0x4000000 cmp=com.android.music/.MediaPlaybackActivity} from uid 10035 on display 0
D/InitAlarmsService( 1130): Clearing and rescheduling alarms.
E/MediaPlayer( 913): Should have subtitle controller already set
V/PhoneStatusBar( 529): setLightsOn(true)
E/MetadataRetrieverClient( 170): failed to extract an album art
E/MetadataRetrieverClient( 170): failed to extract an album art
E/MetadataRetrieverClient( 170): failed to extract an album art
E/MetadataRetrieverClient( 170): failed to extract an album art
W/CursorWrapperInner( 913): Cursor finalized without prior close()
E/MetadataRetrieverClient( 170): failed to extract an album art
E/MetadataRetrieverClient( 170): failed to extract an album art
I/ActivityManager( 435): Displayed com.android.music/.MediaPlaybackActivity: +290ms
W/AudioTrack( 435): AUDIO_OUTPUT_FLAG_FAST denied by client
V/PhoneStatusBar( 529): DEBUG_MEDIA: Disconnecting from old controller: android.media.session.MediaController@1b491a0f
I/MediaFocusControl( 435): AudioFocus requestAudioFocus() from android.media.AudioManager@1de47f28com.android.music.MediaPlaybackService$3@19f88441
W/AudioTrack( 435): AUDIO_OUTPUT_FLAG_FAST denied by client
D/NuPlayerDriver( 170): start(0x74e0d040)
解決済! 解決策の投稿を見る。
The problem has been resolved.
sound {
compatible = "fsl,imx6q-sabresd-sgtl5000",
"fsl,imx-audio-sgtl5000";
model = "sgtl5000-audio";
cpu-dai = <&ssi2>;//set ssi2 is ok
audio-codec = <&codec>;
audio-routing =
"MIC_IN", "Mic Jack",
"Mic Jack", "Mic Bias",
"Headphone Jack", "HP_OUT";
mux-int-port = <2>;
mux-ext-port = <3>;
};
The problem has been resolved.
sound {
compatible = "fsl,imx6q-sabresd-sgtl5000",
"fsl,imx-audio-sgtl5000";
model = "sgtl5000-audio";
cpu-dai = <&ssi2>;//set ssi2 is ok
audio-codec = <&codec>;
audio-routing =
"MIC_IN", "Mic Jack",
"Mic Jack", "Mic Bias",
"Headphone Jack", "HP_OUT";
mux-int-port = <2>;
mux-ext-port = <3>;
};
Hi Shannon,
Thanks for sharing your solution with the Community!
Best regards!
/Carlos
kernel dmesg:
ALSA device list:
#0: sgtl5000-audio
android logcat:
I/AudioPolicyService( 170): AudioPolicyService CSTOR in new mode
I/AudioPolicyManager( 170): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf
W/audio_hw_primary( 170): card 0, id sgtl5000audio ,driver sgtl5000-audio, name sgtl5000-audio
W/audio_hw_primary( 170): out rate 44100