I'm trying to integrate a browser to my yocto rootfs, I am using linuxfb as the platform and not x11 or wayland which makes adding chromiuim browser impossible (please correct me if I'm wrong).
Therefore on trying to add qtwebengine:
I modified my local.conf with the line
IMAGE_INSTALL_append = "qtwebengine"
and now built the rootfs using:
bitbake fsl-image-qt5-validation-imx
but it throws an error saying
ERROR: Task (~/yocto_4_9_88_qt/imx-yocto-bsp/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_compile) failed with exit code '1
I've installed all necessary packages as mentioned in iMX_Yocto_Project_User_guide
do I need to modify the qtdeclarative_git.bb file?
I've attached the error log and the.bb file please have a look.
 
					
				
		
Nope same error is there any other way to get a browser working on linuxfb platform?
 
					
				
		
 gusarambula
		
			gusarambula
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Sujay S,
Have you tried with the configuration shared on the following thread?
https://community.nxp.com/message/1064884?commentID=1064884#comment-1064884
Please let us know if the problem continues.
Regards,