Dear All,
I am using imx25 board where having two ethernet adapter one is from debug and another one is from personality board.
now i am load the file through nfs using debug board adapter. after loaded os fully then i give the ifconfig -a command to work with
personality board eth adapter . it is showing like below. how can i use the on board eth adapter for my use. the problem is eth0 doesnt have Hwaddr and ip and etc .
how can i activate it ?
eth0 | Link encap:Ethernet HWaddr 00:00:00:00:00:00 |
BROADCAST MULTICAST MTU:1500 Metric:1 | |
RX packets:0 errors:0 dropped:0 overruns:0 frame:0 | |
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 | |
collisions:0 txqueuelen:1000 | |
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) | |
Base address:0xa000 |
eth1 | Link encap:Ethernet HWaddr 00:04:9F:00:F6:21 |
inet addr:10.169.42.100 Bcast:10.255.255.255 Mask:255.0.0.0 | |
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 | |
RX packets:2897 errors:0 dropped:171 overruns:0 frame:0 | |
TX packets:1882 errors:0 dropped:0 overruns:0 carrier:0 | |
collisions:0 txqueuelen:1000 | |
RX bytes:2542760 (2.4 MiB) TX bytes:321928 (314.3 KiB) |
Please some one give me the solution ASAP.
Regards,
Guru
Hi i tried the above things but terminal get hanging ...please give some solution ..
Can you try the following?:
1) sudo gedit /etc/network/interfaces
2) you should see the following:
auto eth0
iface eth0 inet dhcp
3) add a line with the new macadress right after the lines in step 2:
hwaddress ether 01:02:03:04:05:06
4) sudo /etc/init.d/networking restart
let me know if it works...