How to add imx8mp HDMI driver in uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add imx8mp HDMI driver in uboot

1,553件の閲覧回数
darshan_kukadiya
Contributor I

I have phycore-imx8m plus board, i have build uboot 20.04 stand alone.

so, How can i add or enable HDMI driver in u-boot?

0 件の賞賛
返信
3 返答(返信)

1,523件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @darshan_kukadiya

Thank you for contacting NXP Support.

Based on the following thread that functionality is unsupported on the i.MX8MP.
Re: Support U-Boot splash screen to kernel in imx8MP for Linux NXP - NXP Community

Have a great day!

 

0 件の賞賛
返信

1,203件の閲覧回数
sunannan
Contributor II

@brian14 

 您好:

         imx8mp的uboot为什么不支持HDMI显示?我在尝试移植HDMI驱动,如果是cpu硬件导致无法在uboot阶段无法显示,能说明原因吗?我的需求是使用HDMI屏幕在3秒左右显示logo。

1,197件の閲覧回数
darshan_kukadiya
Contributor I
exactly the same thing i wanted to do .want to show logo in boot time on HDMI display for imx8mp.
0 件の賞賛
返信