How to add audio driver to IMX53qsb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add audio driver to IMX53qsb

720 Views
prannoy
Contributor I

Hi,

I am using IMX53 qsb board. I want add a new audio driver to the kernel.

kernel version is 2.6.35.

I have source code of that audio driver, I want to add over the spi interface.

Can you please help me.

0 Kudos
Reply
2 Replies

624 Views
fabio_estevam
NXP Employee
NXP Employee

Audio via sgtl5000 codec works by default o FSL kernel or mainline kernel.

0 Kudos
Reply

624 Views
igorpadykov
NXP Employee
NXP Employee

Hi prannoy

please check Chapter 21 "Porting Audio Codecs to a Custom Board"

MX53UG

However before porting I would suggest to check hardware and codes with OBDS

On-Board Diagnostic Suit for the i.MX53 Quick Start Board

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply