How to add a new board to imx28 yocto build?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add a new board to imx28 yocto build?

3,018 Views
Colin_MTData
Contributor III

Hi,   (re-posted from wrong group)

  We have our own hardware based on the imx28evk.  I have built systems for it using LTIB but we want to upgrade to Yocto and to a recent kernel.

I have installed Yocto and built a successfully target for the imx28evk using Yocto.

Now I want to understand how to build for our target hardware.

I have made a little progress, I have added a layer and it is included in the layers seen by bitbake.

  The next thing I want to change is the device tree.  Searching the internet yields many different suggestions.

I have set KERNEL_DEVICETREE = "mtd4000.dtb" in the machine conf file but when I try "bitbake core-image-minimal" it fails trying to build mtd4000.dtb: No rule to build target.

I can't work out where I'm supposed to put the dts files and how to tell the system where they are.

Referring to my workspace below,

1) Can anyone explain where to put the .dts/.dtsi files?

Which path is correct:

    .../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/...

or  .../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/image/usr/...

or some other path?

2) How do I tell Yocto/bitbake about the new .dts file(s)? 

3) If the .dtb has to have an entry in a makefile in the list for the MXS, eg:  "dtb-$(CONFIG_ARCH_MXS) += mtd4000.dtb", how do I do that using my layer?

There is a Makefile in "tmp/work/mtd4000-poky-linux-gnueabi/linux-fslc/3.14+gitAUTOINC+00e472111a-r0/git/arch/arm/boot/dts/Makefile" but

it is replaced when I clean and re-build the target (As I would expect: stuff under 'tmp/...' is transient)

4) Also, I will need to get the "defconfig" right for this new machine.  Where does it go and how to tell Yocto/bitbake ?

     .../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/defconfig

or  .../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/mtd4000/defconfig

There is a SRC_URI in linux-fslc.inc that refers to "file://defconfig" but I don't know which directory this implies?

[ 5) Later I'll need to change the DDR RAM settings and then build u-boot too ]

Thanks in advance,

Colin Moloney

-----------

My build workspace is called "mdtata", my layer is "meta-mtdata" and my new machine is "mtd4000".  My workspace is like:

.../help/

.../mtdata/

.../README

.../README.cm

.../.repo/

.../setup-environment.../download

.../sources/base/

.../sources/meta-fsl-arm/

.../sources/meta-fsl-arm-extra/

.../sources/meta-fsl-demos/

.../sources/meta-openembedded/

.../sources/poky/

and my layer

.../sources/meta-mtdata/

.../sources/meta-mtdata/README

.../sources/meta-mtdata/recipes-kernel/

.../sources/meta-mtdata/recipes-kernel/linux/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc.inc

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc_3.14.bbappend

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/arch/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/arch/arm/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/arch/arm/boot/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/arch/arm/boot/dts/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/3.14/git/arch/arm/boot/dts/mtd4000.dts

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/defconfig

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/mtd4000/

.../sources/meta-mtdata/recipes-kernel/linux/linux-fslc/mtd4000/defconfig

.../sources/meta-mtdata/recipes-bsp/

.../sources/meta-mtdata/recipes-bsp/u-boot/

.../sources/meta-mtdata/recipes-bsp/u-boot/u-boot-fslc.inc

.../sources/meta-mtdata/recipes-bsp/u-boot/u-boot-fslc_2014.01.bb

.../sources/meta-mtdata/recipes-bsp/u-boot/u-boot-mtd4000/

.../sources/meta-mtdata/conf/

.../sources/meta-mtdata/conf/machine/

.../sources/meta-mtdata/conf/machine/mtd4000.conf

.../sources/meta-mtdata/conf/layer.conf

and build directory:

.../mtdata/bitbake.lock

.../mtdata/cache/

.../mtdata/state-cache

.../mtdata/conf/

.../mtdata/conf/local.conf

.../mtdata/conf/templateconf.cfg

.../mtdata/conf/sanity_info

.../mtdata/conf/bblayers.conf

.../mtdata/tmp/

My machine config mtd4000.conf has:

    include conf/machine/include/mxs-base.inc

    PREFERRED_PROVIDER_virtual/kernel = "linux-fslc"

    PREFERRED_VERSION_linux-fslc = "3.14%"

    IMXBOOTLETS_MACHINE = "MTD4000"

    KERNEL_IMAGETYPE = "uImage"

and several attempts at the device tree:

    #KERNEL_DEVICETREE = "imx28-evk.dtb"   -- original freescale

none of these worked:

    KERNEL_DEVICETREE = "mtd4000.dtb"

    KERNEL_DEVICETREE = "${S}/git/arch/arm/boot/dts/mtd4000.dtb"

    KERNEL_DEVICETREE = "${WORKDIR}/mtd4000.dts"

    KERNEL_DEVICETREE = "${WORKDIR}/mtd4000"

The local.conf has:

    MACHINE ??= "mtd4000"

The layer "linux-fslc.inc" is:

    LICENSE = "GPLv2"

    LIC_FILES_CHKSUM = "file://COPYING;md5=d7810fab7487fb0aad327b76f1be7cd7"

    DEPENDS += "lzop-native bc-native"

    PROVIDES = "virtual/kernel linux-mainline"

    inherit kernel

    require recipes-kernel/linux/linux-imx.inc

    require recipes-kernel/linux/linux-dtb.inc

    SRCBRANCH ?= ""

    SRC_URI = "git://github.com/Freescale/linux-mainline.git;branch=${SRCBRANCH} \

               file://defconfig"

    LOCALVERSION = "-fslc"

The layer "linux-fslc_3.14.bbappend" is:

  # Which of these to supply a path to the .dts (and/or the defconfig)?

    FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:"

    FILESEXTRAPATHS_prepend := "${THISDIR}:${THISDIR}/mxs:"

    FILESEXTRAPATHS_prepend := "${THISDIR}/${PN}:${THISDIR}/mxs:${THISDIR}/${PN}/${PV}/git/arch/arm/boot/dts:"

    COMPATIBLE_MACHINE_mtd4000 = "mtd4000"      # Should this be appended or assigned ?

    KMACHINE_mtd4000 = "mtd4000"

Labels (2)
Tags (3)
2 Replies

1,331 Views
fabio_estevam
NXP Employee
NXP Employee

I would recommend:

1. Add support for your board to U-boot

2. Add a dts for your board

Make sure you can boot the kernel.

Then you add it into Yocto.

1,331 Views
gusarambula
NXP TechSupport
NXP TechSupport

I would suggest looking at other machines available as part of the community bsp for reference.

There is a set of slides that may be of help here (please note that you may need to login to download it), the kernel tree information is on slide 28.

http://www.freescale.com/webapp/Download?colCode=FTF-SDS-F0106&Parent_nodeId=131741541207669681D199&...

Besides that you must also include your .dtb file in the Makefile in the dts source folder, in the CONFIG_ARCH_MXC section. This was once addressed in some discussion list but was not added to the slides.

I hope this information helps!

0 Kudos
Reply