How to add a new LCD driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add a new LCD driver

466 Views
road_wang
Contributor I

     Refer to attachment panel specification,I‘m add a new LCD driver。The following files have been changed,But the screen doesn't show anything, only the backlight is on,Is there any other file to change?

 1、arch/arm/boot/dts/imx6ul-14x14-evk.dts:

&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat
&pinctrl_lcdif_ctrl>;
display = <&display0>;
status = "okay";

display0: display {
bits-per-pixel = <16>;
bus-width = <24>;

display-timings {
native-mode = <&timing0>;
timing0: timing0 {
mode_name = "TFT70AB-800x480";
clock-frequency = <33000000>;
hactive = <800>;
vactive = <480>;
hfront-porch = <121>;
hback-porch = <88>;
hsync-len = <48>;
vback-porch = <39>;
vfront-porch = <21>;
vsync-len = <3>;

hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <0>;
};
};
};
};

2. board\freescale\imx6ul_14x14_evk\imx6ul_14x14_evk:

struct display_info_t const displays[] = {{
.bus = MX6UL_LCDIF1_BASE_ADDR,
.addr = 0,
.pixfmt = 24,
.detect = NULL,
.enable = do_enable_parallel_lcd,
.mode = {
.name = "TFT70AB-800x480",
.xres = 800,
.yres = 480,
.pixclock = 30303,
.left_margin = 48,
.right_margin = 121,
.upper_margin = 39,
.lower_margin = 21,
.hsync_len = 88,
.vsync_len = 3,
.sync = 0,
.vmode = FB_VMODE_NONINTERLACED

} } };

0 Kudos
1 Reply

364 Views
igorpadykov
NXP Employee
NXP Employee

Hi road

one can recheck lcd power up sequence defined in sect.3.2. Power Sequence

and test it for example in uboot, function do_enable_parallel_lcd()

mx6ul_14x14_evk.c\mx6ul_14x14_evk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos