How to add RTC(ds1307) in i.mx25 Linux kernel 2.6.31 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add RTC(ds1307) in i.mx25 Linux kernel 2.6.31 ?

2,095 Views
gurumoorthirasi
Contributor IV

Dear All,

I am using i.mx25 processor for our application.I am using Linux 2.6.31 with freescale BSP for i.mx25. we require RTC for our application.

Any one tel me what are changes involved in kernel 2.631 to add RTC(Ds1307) and work it up.

Regards,

Guru

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

1,786 Views
b36401
NXP Employee
NXP Employee

Please refer to section 26.5 "Programming Interface" of attached Linux manual regarding to supported RTC API functions for i.MX25 processor.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply