How to add HDMI and LCD both(Dual display) on latest devicetree supported kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add HDMI and LCD both(Dual display) on latest devicetree supported kernel

Jump to solution
5,671 Views
narasimhuluorug
Contributor III

Hi,

Any one can guide me how to add dual display support on latest kernel with devicetree based on imx6 sabreSD target. I need to create on same two frame buffers needed to support this too.

Thanks in advance.

Thanks & Regards,

Narasimha.

Labels (5)
0 Kudos
Reply
1 Solution
3,873 Views
igorpadykov
NXP Employee
NXP Employee

Hi narasimhulu

dual display is supported by BSP as described on p.23 attached Linux

Guide "Specifying displays", for dts files one can look at sources:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=im...

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q-sabresd.dts...

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q.dtsi?h=imx_...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,874 Views
igorpadykov
NXP Employee
NXP Employee

Hi narasimhulu

dual display is supported by BSP as described on p.23 attached Linux

Guide "Specifying displays", for dts files one can look at sources:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl.dtsi?h=im...

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q-sabresd.dts...

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q.dtsi?h=imx_...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,873 Views
narasimhuluorug
Contributor III

Hi Igor,

Can you give information regarding the dual display issue with 3.19 kernel if available so. I am working on 3.19 kernel i found lot changes from 3.14 to 3.19. If you have any information please share your suggestions.

Thanks in Advance,

Narasimha

0 Kudos
Reply
3,873 Views
fabio_estevam
NXP Employee
NXP Employee

This patch allows HDMI and LVDS to be used at the same time on a mx6sabresd:

https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/commit/arch/arm/boot/dts/imx6qd...

I would suggest you to try a more recent kernel though.

Regards,

Fabio Estevam

0 Kudos
Reply
3,873 Views
narasimhuluorug
Contributor III

Hi Fabio,

Thanks for the information but before this applying patch we need to create multiple frame buffers. How to achieve this on this 3.19 kernel or above. As i have scene drivers directory structure has changed compare with 3.14 to 3.19 kernel.

Thanks & Regards,

Narasimha

0 Kudos
Reply
3,873 Views
narasimhuluorug
Contributor III

Hi Igor,

Thank you very much for sharing this information. But I want use 3.19 kernel with devicetree supported dualdisplay. If have any information please share me on the same.

Best Regards,

Narasimha

0 Kudos
Reply