How to add Ethernet settings to JB4.2 on imx6 sabresd?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add Ethernet settings to JB4.2 on imx6 sabresd?

1,114 Views
jiangshao
Contributor V

I want to add Ethernet settings ( for example : static IP) to JB4.2. What should I do ?
I have made ​​reference to theHow to Add Ethernet UI Support in ICS,

but those patches are made for JB4.0 , the direct use will be a lot of errors.

Labels (3)
0 Kudos
1 Reply

430 Views
SergioSolis
NXP Employee
NXP Employee

Hello Jiang,

In the same thread you mention, at the end of the very first post, the engineer mentions that they created an APK for 4.2 and 4.3. It is not a direct UI but an APK , though it works.

0 Kudos