How to adapt my BSP for a new audio codec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to adapt my BSP for a new audio codec

1,398 Views
fredericjary
Contributor I

Hello,

I am working on a custom board, whose reference design is Sabre SDB board.

I would like to port a new codec (max98355a) on my board. Compared to wm8962 codec from the reference board, this codec has no I2C as a control interface. As the registration of the device is done via I2C interface on the wm8962, the wm8962.c driver shall be modified, and also the imx-8962.c file. For the moment, the probe of the codec driver fails.

Does anybody knows what is the main idea to modify the driver files to force probing without I2C polling? There are not so many examples of codec drivers in Linux source code so that I can get inspired...

Any idea would be very appreciated.

Thank you.

Labels (3)
0 Kudos
Reply
2 Replies

804 Views
YuryGeorgievski
Contributor I

Hello Frederic,

So did you implement/find max98355 driver?

I need to integrate it as well in my custom board.

Do you know what is the closest/best already existing max98*.c drivers that can be used

as a base for max98355 implementation?

Thanks for help.

0 Kudos
Reply

804 Views
fabio_estevam
NXP Employee
NXP Employee

First of all you need to create a codec driver for max98355.

Using wm8962 as reference would not help in this case.

Take a look at existing  maxim codec drivers as reference:

ls  sound/soc/codecs/max98*.c

sound/soc/codecs/max98088.c  sound/soc/codecs/max9850.c

sound/soc/codecs/max98090.c  sound/soc/codecs/max9877.c

sound/soc/codecs/max98095.c


,and then adapt it to max98355a.

A good place to discuss this is alsa-devel mailing list.

0 Kudos
Reply