How to activate PCIe Data_Link_Layer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to activate PCIe Data_Link_Layer

1,487 次查看
george
Senior Contributor II

Dear all,

We want to use PCIe on i.MX6.

The method of generate the Configuration Cycle is being known gradually.

Currently, the method of setting Data Link Layer to Active is investigated.

To this, I think that setting is required in an order from the physical layer.

Please recommend, if there are materials which are consulted.

And, which around in Source of Linux should be seen?

Best Regards,

George

标记 (3)
0 项奖励
回复
2 回复数

1,283 次查看
igorpadykov
NXP Employee
NXP Employee

Hi George, most suitable way to run SDK PCIe

example, please read included in package

iMX6_Firmware_Guide.pdf. Linux "L3.0.35_4.1.0_ER_SOURCE"

package can be found on the same link, in Linux package please read

i.MX_6Dual6Quad_Linux_Reference_Manual.pdf

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

One can run tests from iRAM using scripts below

iRAM (OCRAM) i.MX6 SDK Application

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,283 次查看
george
Senior Contributor II

Dear Chip,

I try to look for required information from the materials which you showed.

And it will post again here, when there is a question.

Thanks

Best Regards,

George

0 项奖励
回复