How to achieve VGA hot plug for i.mx6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to achieve VGA hot plug for i.mx6?

710 Views
dingyanhong
Contributor I

Our product is based on mx6D, and we use RGB interface transfer to VGA。

we need VGA hot plug function, do not power off mx6, when we plug VGA display, the system can read EDID and set to the suitable resolution according to the EDID.

is there any solution to accomplish this function?thanks!

Labels (1)
0 Kudos
Reply
1 Reply

553 Views
Pavel
NXP Employee
NXP Employee

Specification of VGA does not support hot plug possibility. Therefore there is no similar solution.

Look at HDMI possibility. HDMI supports hot plugging (http://en.wikipedia.org/wiki/HDMI).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------