I have created ext3 partition with rootfs in it.
I have created fat partition and saved a file in it on my host pc.
Now, I have put my SD card in board, I am able to browse through all my files on ext3, then how to access files on the fat partition.
I use minicom to boot u-boot in linux.
Version 10.04 LTS Ubuntu.
Regards Krishna Pavan
Hi Daiane, I must thank you for remembering me my thread.
Here I am posting the solution to that thread.
make directory in /mnt/YOUR_MOUNT_POINT for example
Then use this command.
mount -t vfat -o iocharset=utf8,umask=0022 /dev/mmcblk0p2 /mnt/YOUR_MOUNT_POINT
If its a ntfs/ext2/3/4, then the specific iocharset/ can be used
for ntfs
# sudo mount -t ntfs -o nls=utf8,umask=0222 /dev/hdb1 /media/c
umask can be obtained from the command in the help commands in terminal.
/dev/hdb1 is your device that can be obtained from "fdisk -l devicename" or "cat /proc/partitions"
we will get an iocharset error, but can be ignored if we are not using it on windows.
Regards :: Krishna Pavan
Yeah, yea Daiane,
I have solved that, We have to create a mountpoint in the /dev/ and then using the commands specific to the OS inside the U-boot that is loaded, we have to mount the partition. I have got it right, after many attempts, finally it o.k now.
Regards Krishna Pavan
Hi.
Both partition are on the same SDCard?
You should to mount the fat partition on some /mnt dir.
take a look on dmesg in order to see which /dev/XXX you should take