How to access QSPI flash in i.MX8MPlus EVK on Windows 10 IoT Enterprise

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to access QSPI flash in i.MX8MPlus EVK on Windows 10 IoT Enterprise

769件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

 

We would like to test QSPI flash access with Windows 10 IoT Enterprise.

According to the following thread, we seems that it can be access QSPI flash by default BSP.

Solved: Re: QSPI flash support on Windows 10 IoT Enterprise - NXP Community

 

I tried with EVK, but could not see the QSPI flash in the Windows device list.

It seems that QSPI hardware information is not up on the Windows OS side from UEFI.

 

Q1.

Is there a Windows driver provided to access QSPI?

 

Q2.

How can we access QSPI flash on EVK with Windows 10 IoT Enterprise ?

 

Ko-hey

0 件の賞賛
返信
1 返信

676件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

QSPI flash is only supported in Uboot and UEFI. Windows driver is not supported but is available via UEFI variables features.

More information here: 

\mu_platform_nxp\Silicon\ARM\NXP\iMX8Pkg\Drivers\iMXNorFlashDxe\README.txt

Best regards.

0 件の賞賛
返信