Hi All,,,
I want to reduce the booting time. and i am using the imx6dl Sabreauto board and kernel version is 3.14.28 and image name is " fsl-image-qt5 " from yocto, for reducing the booting time i followed some links but it wont work for me, On 13th second i am getting the my application window, so i want to reduce that time within 6 to 7 second i want see my application window,
here is the i followed some links:
Linux Fast Boot on i.MX6 Sabresd Board
Hi, Fast Bootup time for imx6Q sabre auto board.
https://community.nxp.com/docs/DOC-94738
https://community.nxp.com/message/895274?commentID=895274#comment-895274
And i disable the some modules(driver) in my kernel using "menuconfig" which is i am not using. The size of zImage is little bit reduced but no change in the booting time, can any one help me how solve this issue.
Thanks In Advance,
Best Regards.
Nandish SG