How to Read 17 bytes continually from i2c slave in imx6 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Read 17 bytes continually from i2c slave in imx6 processor

ソリューションへジャンプ
2,156件の閲覧回数
ayyappadasps
Contributor II

hi all;

        i want to read 17bytes continually from a slave i2c device.

       i am getting an error saying the "host stop reading before 17 bytes" from status flag

    How to slove it?###

ラベル(4)
0 件の賞賛
返信
1 解決策
1,973件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ayyappadas

please check

Variable-length I2C messages 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,974件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ayyappadas

please check

Variable-length I2C messages 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,973件の閲覧回数
ayyappadasps
Contributor II

 Thankyou  igorpadykov

                              I was able to solve the issue

0 件の賞賛
返信