How to Enable FlexCAN in device tree on iMX6QP custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Enable FlexCAN in device tree on iMX6QP custom board

8,501 Views
kishorr
Contributor II

I am trying to enable FlexCAN bus 1 and 2 on iMX6QP based custom hardware.
The two CAN buses are connected from iMX6 as below

GPIO_7    : CAN-TX1
GPIO_8    : CAN-RX1
GPIO-4-5  : CAN-STBY1

KEY_COL4 : CAN-TX2
KEY_ROW4 : CAN-RX2
GPIO-6-10 : CAN-STBY2

The device tree is defined as below:
arch/arm/boot/dts/imx6qdl.dtsi
================================

/ {
        aliases {
                flexcan0 = &flexcan1;
                flexcan1 = &flexcan2;
                gpio0 = &gpio1;
...
...

  soc {
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "simple-bus";
                interrupt-parent = <&intc>;
                ranges;

                caam_sm: caam-sm@00100000 {
                        compatible = "fsl,imx6q-caam-sm";
                        reg = <0x00100000 0x3fff>;
                };

     flexcan1: can@02090000 {
                                compatible = "fsl,imx6q-flexcan";
                                reg = <0x02090000 0x4000>;
                                interrupts = <0 110 IRQ_TYPE_LEVEL_HIGH>;
                                clocks = <&clks IMX6QDL_CLK_CAN1_IPG>,
                                         <&clks IMX6QDL_CLK_CAN1_SERIAL>;
                                clock-names = "ipg", "per";
                                stop-mode = <&gpr 0x34 28 0x10 17>;
                                status = "enabled";
                        };

    flexcan2: can@02094000 {
                                compatible = "fsl,imx6q-flexcan";
                                reg = <0x02094000 0x4000>;
                                interrupts = <0 111 IRQ_TYPE_LEVEL_HIGH>;
                                clocks = <&clks IMX6QDL_CLK_CAN2_IPG>,
                                         <&clks IMX6QDL_CLK_CAN2_SERIAL>;
                                clock-names = "ipg", "per";
                                stop-mode = <&gpr 0x34 29 0x10 18>;
                                status = "enabled";
                        };


arch/arm/boot/dts/imx6q.dtsi
=====================

&flexcan1 {
                 pinctrl_flexcan1_1: flexcan1grp {
                fsl,pins = <
                        MX6QDL_PAD_GPIO_7__FLEXCAN1_TX          0x1b0b0
                        MX6QDL_PAD_GPIO_8__FLEXCAN1_RX          0x1b0b0
                >;
        };
};


&flexcan2 {
        pinctrl_flexcan2_1: flexcan2grp {
                fsl,pins = <
                        MX6QDL_PAD_KEY_COL4__FLEXCAN2_TX        0x1b0b0
                        MX6QDL_PAD_KEY_ROW4__FLEXCAN2_RX        0x1b0b0
                >;
        };

};

arch/arm/boot/dts/imx6q-sabresd.dts
===================================

&flexcan1 {

         status = "okay";
};

&flexcan2 {

         status = "okay";
};

I observe CAN0 and CAN1 interfaces are up.
root@QPU2:~# ifconfig can0
can0      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  
          UP RUNNING NOARP  MTU:16  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:10
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:142


root@QPU2:~# ifconfig can1
can1      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  
          UP RUNNING NOARP  MTU:16  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:10
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:143

I have connected both the CAN ports to KOMODO CAN analyser. When I send packets I do not see any packets sent out from either of the ports. I have run the internal loopback test which is successful.

ip link set can0 up type can bitrate 125000
ifconfig can0 up
ifconfig can0
cansend can0 100#1122334455667788

I suspect some issue with the device tree configuration. Appreciate if anyone could provide some pointers to the problem I am facing.

Thanks
Kishor

0 Kudos
Reply
8 Replies

5,363 Views
kishorr
Contributor II

Hi Igor,

The issue is resolved, It turns out to be the pinctrls are not placed inside the iomuxc node in dtsi file.

Thanks you.

Kishor

0 Kudos
Reply

5,363 Views
rogerlee0212
Contributor I

Hi  kishor 

      Can U share your  dtsi file ?

      

      my flexcan on MCIMX6Q-SDB  RevC4   doesn't work, what should I do now? 

---------------------

U-Boot 2014.04-08637-gaffa032 (Dec 01 2016 - 12:25:25)

CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 22 C, calibration data: 0x5a04f57d#
Reset cause: POR
Board: MX6-SabreSD

-----------------------------

Linux version 3.10.17 (root@localhost-desktop) (gcc version 4.8.3 20140401 (prerelease) (crosstool-NG linaro-1.13.1-4.8-2014.04 - Linaro GCC 4.8-2014.04) ) #12 SMP PREEMPT Mon Oct 24 11:34:41 CST 2016

---------------------------------------

[/] # dmesg |grep can
pci_bus 0000:00: scanning bus
pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0
pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1
pci_bus 0000:01: scanning bus
pci_bus 0000:01: bus scan returning with max=01
pci_bus 0000:00: bus scan returning with max=01
ahci: SSS flag set, parallel bus scan disabled
flexcan 2090000.can: device registered (reg_base=c0a68000, irq=142)
can: controller area network core (rev 20120528 abi 9)
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
[/] # /bin/ip link set can0 up type can bitrate 5000
flexcan 2090000.can can0: writing ctrl=0xf93e2007
[/] # ifconfig can0
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:142

[/] #

[/] # /bin/ip -s -d link show can0
2: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN qlen 10
link/can
can state ERROR-ACTIVE (berr-counter tx 0 rx 0) restart-ms 0
bitrate 5000 sample-point 0.708
tq 8333 prop-seg 8 phase-seg1 8 phase-seg2 7 sjw 1
flexcan: tseg1 4..16 tseg2 2..8 sjw 1..4 brp 1..256 brp-inc 1
clock 30000000
re-started bus-errors arbit-lost error-warn error-pass bus-off
0 0 0 0 0 0
RX: bytes packets errors dropped overrun mcast
0 0 0 0 0 0
TX: bytes packets errors dropped carrier collsns
0 0 0 0 0 0
[/] # /bin/ip -s -d link show can0
2: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN qlen 10
link/can
can state ERROR-WARNING (berr-counter tx 0 rx 129) restart-ms 0
bitrate 5000 sample-point 0.708
tq 8333 prop-seg 8 phase-seg1 8 phase-seg2 7 sjw 1
flexcan: tseg1 4..16 tseg2 2..8 sjw 1..4 brp 1..256 brp-inc 1
clock 30000000
re-started bus-errors arbit-lost error-warn error-pass bus-off
0 0 0 1 0 0
RX: bytes packets errors dropped overrun mcast
8 1 0 0 0 0
TX: bytes packets errors dropped carrier collsns
0 0 0 0 0 0
[/] # /opt/imx6/app/can/cansend can0 100#1122334455667788
interface = can0, family = 29, type = 3, proto = 1
[/] #
[/] #
[/] # /bin/ip -s -d link show can0
2: can0: <NO-CARRIER,NOARP,UP,ECHO> mtu 16 qdisc pfifo_fast state DOWN qlen 10
link/can
can state BUS-OFF (berr-counter tx 0 rx 0) restart-ms 0
bitrate 5000 sample-point 0.708
tq 8333 prop-seg 8 phase-seg1 8 phase-seg2 7 sjw 1
flexcan: tseg1 4..16 tseg2 2..8 sjw 1..4 brp 1..256 brp-inc 1
clock 30000000
re-started bus-errors arbit-lost error-warn error-pass bus-off
0 0 0 1 1 1
RX: bytes packets errors dropped overrun mcast
24 3 0 0 0 0
TX: bytes packets errors dropped carrier collsns
0 0 0 0 0 0
[/] #

--------------------debugfs info-----------------------

9 mount -t debugfs none /sys/kernel/debug/
10 cd /sys/kernel/debug/
11 ll
12 cd pinctrl/
13 ll
14 cd 20e0000.iomuxc/
15 ll
16 cat pinconf-pins
17 cat pinmux-pins
18 cat pinmux-functions
19 cat pins
20 cat pingroups
21 cat pinconf-groups
22 cat pinconf-config
23 cat gpio-ranges

pin 149 (MX6Q_PAD_GPIO_19):0x1b0b0

pin 144 (MX6Q_PAD_GPIO_7): 2090000.can (GPIO UNCLAIMED) function flexcan1 group flexcan1grp
pin 145 (MX6Q_PAD_GPIO_8): 2090000.can (GPIO UNCLAIMED) function flexcan1 group flexcan1grp

pin 149 (MX6Q_PAD_GPIO_19): 2090000.can (GPIO UNCLAIMED) function flexcan1 group flexcan1grp


function: flexcan1, groups = [ flexcan1grp ]


pin 144 (MX6Q_PAD_GPIO_7) 20e0000.iomuxc
pin 145 (MX6Q_PAD_GPIO_8) 20e0000.iomuxc

pin 149 (MX6Q_PAD_GPIO_19) 20e0000.iomuxc


group: flexcan1grp
pin 144 (MX6Q_PAD_GPIO_7)
pin 145 (MX6Q_PAD_GPIO_8)
pin 149 (MX6Q_PAD_GPIO_19)

0 Kudos
Reply

5,363 Views
rogerlee0212
Contributor I


Finally, we found is that the chip TJA1040T is not working properly.

Flexcan works well after we use SN65HVD233

thx, kishorr

0 Kudos
Reply

5,363 Views
kishorr
Contributor II

I have tested internal loopback and works. Right now I have connected the CAN ports to KOMODO unit.

0 Kudos
Reply

5,363 Views
igorpadykov
NXP Employee
NXP Employee

what is about external loopback, is it working.

0 Kudos
Reply

5,363 Views
kishorr
Contributor II

Thanks igor.

I have updated the device tree files. But still not able to send any packets on can0 or can1 interfaces.

Just providing the device tree info for reference:

arch/arm/boot/dts/imx6q.dtsi:

&flexcan1 {
       pinctrl_flexcan1_1: flexcan1grp-1 {
                fsl,pins = <
                        MX6QDL_PAD_GPIO_7__FLEXCAN1_TX          0x1b0b0
                        MX6QDL_PAD_GPIO_8__FLEXCAN1_RX          0x1b0b0
                        MX6QDL_PAD_GPIO_19__GPIO4_IO05          0x1b0b0
                        >;
                };
};

&flexcan2 {
        pinctrl_flexcan2_1: flexcan2grp-2 {
                fsl,pins = <
                        MX6QDL_PAD_KEY_COL4__FLEXCAN2_TX        0x1b0b0
                        MX6QDL_PAD_KEY_ROW4__FLEXCAN2_RX        0x1b0b0
                        MX6QDL_PAD_NAND_RB0__GPIO6_IO10              0x1b0b0
                        >;
         };

arch/arm/boot/dts/imx6qdl.dtsi:

  flexcan1: can@02090000 {
                                compatible = "fsl,imx6q-flexcan";
                                reg = <0x02090000 0x4000>;
                                interrupts = <0 110 IRQ_TYPE_LEVEL_HIGH>;
                                clocks = <&clks IMX6QDL_CLK_CAN1_IPG>,
                                         <&clks IMX6QDL_CLK_CAN1_SERIAL>;
                                clock-names = "ipg", "per";
                                stop-mode = <&gpr 0x34 28 0x10 17>;
                                status = "disabled";
                        };

                        flexcan2: can@02094000 {
                                compatible = "fsl,imx6q-flexcan";
                                reg = <0x02094000 0x4000>;
                                interrupts = <0 111 IRQ_TYPE_LEVEL_HIGH>;
                                clocks = <&clks IMX6QDL_CLK_CAN2_IPG>,
                                         <&clks IMX6QDL_CLK_CAN2_SERIAL>;
                                clock-names = "ipg", "per";
                                stop-mode = <&gpr 0x34 29 0x10 18>;
                                status = "disabled";
                        };

arch/arm/boot/dts/imx6q-sabresd.dts

&flexcan1 {
         pinctrl-names = "default";
         pinctrl-0 = <&pinctrl_flexcan1_1>;
         trx-stby-gpio = <&gpio4 5 GPIO_ACTIVE_LOW>;
         status = "okay";
};

&flexcan2 {
         pinctrl-names = "default";
         pinctrl-0 = <&pinctrl_flexcan2_1>;
         trx-stby-gpio = <&gpio6 10 GPIO_ACTIVE_LOW>;
         status = "okay";
};

&fec {
        status = "disabled";
};

When I send a packet using cansend utility I see debug messages from flexcan_start_xmit

but flexcan_irq is not getting triggered.

I see below messages in the kernel initialization:

2090000.can supply xceiver not found, using dummy regulator
2094000.can supply xceiver not found, using dummy regulator

we are using 33901 Can Tranceiver.

root@U2:~# ifconfig
can0      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  
          UP RUNNING NOARP  MTU:16  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:10
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:142

can1      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  
          UP RUNNING NOARP  MTU:16  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:10
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)
          Interrupt:143

after sending 10 packets i see the below message

root@U2:~# cansend can0 100#1122334455667788
write: No buffer space available

Any idea whats going on.

Thanks

Kishor

0 Kudos
Reply

5,363 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kishor

is it working with loopback test, as without connection can to
some another can, it will not work (it will consider line as busy).

Best regards
igor

0 Kudos
Reply

5,363 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kishor

can is used on sabre ai board and one can check imx6qp-sabreauto-flexcan1.dts, imx6qdl.dtsi settings:
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qdl.dtsi?id=rel_i...
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx6qp-sabreauto-flex...


test details are described in imx-test (folder ..test/can)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply