CONFIG_IMX2_WDT=y
CONFIG_IMX_SC_WDT=y
CONFIG_HAVE_ARM_SMCCC=y
CONFIG_IMX_SCU=y
CONFIG_WATCHDOG=y
CONFIG_WATCHDOG_CORE=y
CONFIG_WATCHDOG_HANDLE_BOOT_ENABLED=y
CONFIG_WATCHDOG_OPEN_TIMEOUT=0
Hi @krsuresh
Default BSP has enabled the watchdog, and NXP provides test demo in BSP.
root@imx8mpevk:/unit_tests/Watchdog# ls
README autorun-wdog.sh dbg_monitor.sh wdt_driver_test.out
root@imx8mpevk:/unit_tests/Watchdog# ./wdt_driver_test.out
---- Running < ./wdt_driver_test.out > test ----
Usage: wdt_driver_test <timeout> <sleep> <test>
timeout: value in seconds to cause wdt timeout/reset
sleep: value in seconds to service the wdt
test: 0 - Service wdt with ioctl(), 1 - with write()
Source code:
https://github.com/nxp-imx/imx-test/blob/lf-5.15.32_2.0.0/test/wdog/wdt_driver_test.c
Test:
root@imx8mpevk:/unit_tests/Watchdog# ./wdt_driver_test.out 10 10 10
---- Running < ./wdt_driver_test.out > test ----
Starting wdt_driver (timeout: 10, sleep: 10, test: write)
Trying to set timeout value=10 seconds
The actual timeout was set to 10 seconds
Now reading back -- The timeout is 10 seconds
U-Boot SPL 2023.04-lf_v2023.04+g49b102d988 (Nov 21 2023 - 07:28:53 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x0, pagesize 0x200, ivt offset 0x0
NOTICE: Do not release JR0 to NS as it can be used by HAB
NOTICE: BL31: v2.8(release):android-14.0.0_1.0.0-rc1-1-g08e9d4eef
NOTICE: BL31: Built : 06:43:30, Nov 21 2023
Best Regards
Zhiming