How to Accurately Count Encoder Pulses on i.MX93 Without Missing Pulses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Accurately Count Encoder Pulses on i.MX93 Without Missing Pulses

1,004件の閲覧回数
dhruvinrajpura
Contributor III

Hello,

 

I am using the i.MX93 11X11 EVK and need to interface motor encoder in A core. Each encoder has two output signals (A and B), where A pin track the Pulse Count and B pin used to find the Direction of Motor and I need to accurately count the pulses to track motor movement and direction.

My main requirement is to ensure no pulses are missed, even at higher speeds. Could you please suggest the best way to achieve this on the i.MX93 11x11 EVK?

タグ(1)
0 件の賞賛
返信
1 返信

984件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @dhruvinrajpura 

I hope you are doing very well.

 

I recommend to you to use the Cortex M33 for this task, and let Cortex A to handle Linux or the Operating system you will use.

If you need to communicate Cortex M33 and Cortex A, you can use RPMSG framework to communicate the cores, exchange data or turn on/off flags.

 

I hope this information can helps to you.

 

Best regards,

Salas.

0 件の賞賛
返信