Hello,
I'm trying to get IR to work in EVK.
- EVK : 8MNANOD4-CPU
- Linux BSP Version : L5.4.3
I already found the article below through a search, but it keeps failing because the board is different.
IMX8 gpio ir receiver using LIRC
Up to now, installing LIRC and checking the version has been successful.
Can you please tell me how to edit the .dts file so that the IR GPIO can be set.
已解决! 转到解答。
unfortunately LIRC and IR are not supported in NXP BSPs, so you should add such support
yourself or apply (if needed) for help to : https://contact.nxp.com/new-prof-svcs-sw-tech
Best regards
igor
Hi Kisu
one can look at example provided on
https://www.imx6rex.com/open-rex/software/how-to-use-access-openrex-peripherals/#ir_rec
Best regards
igor
Hi @igorpadykov ,
I took a closer look at the website you mentioned.
That method was not the Yocto based solution I wanted.
Unfortunately, the directory names and locations didn't work for me, and it was difficult for me to change them.
As already mentioned in the question, the installation of LIRC was successful, and the GPIO settings are not working like the referenced site.
Best Regards,
RabbitThief
unfortunately LIRC and IR are not supported in NXP BSPs, so you should add such support
yourself or apply (if needed) for help to : https://contact.nxp.com/new-prof-svcs-sw-tech
Best regards
igor