How much I.MX27 and MT46H32M32LFCM-75IT (DDR2) with the requirements of the transmission line impedance?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How much I.MX27 and MT46H32M32LFCM-75IT (DDR2) with the requirements of the transmission line impedance?

Jump to solution
947 Views
任贵孙
Contributor II

How much I.MX27 and MT46H32M32LFCM-75IT (DDR2) with the requirements of the transmission line impedance?

I just touched the high-speed signal, please understand!

0 Kudos
1 Solution
742 Views
Yuri
NXP Employee
NXP Employee

1.
  When considering a (i.MX27) PCB design, we may use the next app note as base.

Note, i.MX31 and i.MX27 have similar SDRAM controllers.

"AN3963 :       Interfacing DDR Memories with the i.MX31"

http://cache.freescale.com/files/dsp/doc/app_note/AN3963.pdf


   Strictly speaking to design a high-speed bus, we have to analyze signal rise-

times and trace lengths to see if some termination schemes are needed (to avoid

signal corruption because of reflections).

In order to define termination scheme (and resistor parameters) for signal

termination scheme, the design (board) should be simulated using IBIS / SPICE

models for the device (i.MX27), also actual board trace lengths should be

estimated too.

2.
IMX27 Reference Manual :

http://cache.freescale.com/files/32bit/doc/ref_manual/MCIMX27RM.pdf?fasp=1

Summary Page :

ARM9™ Cores: i.MX27 Processors

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------



View solution in original post

0 Kudos
4 Replies
742 Views
Yuri
NXP Employee
NXP Employee

Strictly speaking, i.MX27 does not support DDR2, sorry.

IMX27 supports only DDR, more accurately LPDDR, please refer to

sect.18.1.9 "Features", i.MX27 Reference Manual.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
742 Views
任贵孙
Contributor II

I'm sorry. I am using a Micron MT46H32M32LFCM-75IT, it is LPDDR. Will they need the transmission line impedance is much ?Will they need the series matching resistor?

I did not find  i.MX27 reference manual in the official website. Do you know the piece in the official website? Can you send me a Web links?

Sorry,my English is poor.

0 Kudos
743 Views
Yuri
NXP Employee
NXP Employee

1.
  When considering a (i.MX27) PCB design, we may use the next app note as base.

Note, i.MX31 and i.MX27 have similar SDRAM controllers.

"AN3963 :       Interfacing DDR Memories with the i.MX31"

http://cache.freescale.com/files/dsp/doc/app_note/AN3963.pdf


   Strictly speaking to design a high-speed bus, we have to analyze signal rise-

times and trace lengths to see if some termination schemes are needed (to avoid

signal corruption because of reflections).

In order to define termination scheme (and resistor parameters) for signal

termination scheme, the design (board) should be simulated using IBIS / SPICE

models for the device (i.MX27), also actual board trace lengths should be

estimated too.

2.
IMX27 Reference Manual :

http://cache.freescale.com/files/32bit/doc/ref_manual/MCIMX27RM.pdf?fasp=1

Summary Page :

ARM9™ Cores: i.MX27 Processors

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------



0 Kudos
742 Views
任贵孙
Contributor II

I'm sorry for my poor English in advance.

0 Kudos