How maximum FPC cable distance should I use for MIPI DSI LCD ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How maximum FPC cable distance should I use for MIPI DSI LCD ?

Jump to solution
3,124 Views
talel_hajsalem
Contributor III

Hello,

I'm working on a custom IMX8MM board, and I have an LCD display.

when using a 5cm FPC cable and its working, but when using 10cm or 20cm it does not work.

If I decrement the pixel clock it sometimes work.

How maximum length should I don't pass?

Thanks,

Talel

Labels (1)
0 Kudos
Reply
1 Solution
3,117 Views
igorpadykov
NXP Employee
NXP Employee

Hi Talel

 

cable length depends on many factors, including cable material, signal losses in board/cable and

connectors, impedance matching, so I am afraid there is no simple formula to calculate. 

One can try to find it experimentally controlling signal quality by oscilloscope or try to perform ibis modelling.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
3,118 Views
igorpadykov
NXP Employee
NXP Employee

Hi Talel

 

cable length depends on many factors, including cable material, signal losses in board/cable and

connectors, impedance matching, so I am afraid there is no simple formula to calculate. 

One can try to find it experimentally controlling signal quality by oscilloscope or try to perform ibis modelling.

 

Best regards
igor

0 Kudos
Reply