How many LPDDR4 can I connect to the iMX8MPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many LPDDR4 can I connect to the iMX8MPlus

Jump to solution
1,052 Views
GuiDas
Contributor II

Hello,

I need an information for the implementation of a *32 LPDDR4 on the iMX8MPlus processor. I calculate that we can only connect 2 of them, limited by the number of DMI, which is 4, on the processor, is my calculation good or can we connect more of them ?

Thank you in advance,

Guilhem

Tags (1)
0 Kudos
Reply
1 Solution
1,046 Views
igorpadykov
NXP Employee
NXP Employee

Hi Guilhem

 

from sect.9.4.1.1 Features i.MX 8M Plus Applications Processor Reference Manual

(Rev. D, 12/2020)

 

• Four ranks supported for DDR4
• Two ranks supported for LPDDR4

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
1,047 Views
igorpadykov
NXP Employee
NXP Employee

Hi Guilhem

 

from sect.9.4.1.1 Features i.MX 8M Plus Applications Processor Reference Manual

(Rev. D, 12/2020)

 

• Four ranks supported for DDR4
• Two ranks supported for LPDDR4

 

Best regards
igor

0 Kudos
Reply