How many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6

1,518件の閲覧回数
ashokp
Contributor I

Hi All,

Please let me know how many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6.

Thanks,

P.Ashok

0 件の賞賛
返信
2 返答(返信)

1,306件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

i.MX6 contains single MIPI CSI to IPU Gasket (CSI2IPU), so one camera can be connected

to it, but  MIPI CSI 2supports up to four concurrent (virtual) channels

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,306件の閲覧回数
kenyung
Contributor I

But there is only one clk lane, how can we seperate one clk lane to two? is there a ic to seperate the clk lane to two ?

0 件の賞賛
返信