How many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6

1,005 Views
ashokp
Contributor I

Hi All,

Please let me know how many CSI-2(MIPI) cameras can be interfaced simultaniously in IMX6.

Thanks,

P.Ashok

0 Kudos
Reply
2 Replies

793 Views
Yuri
NXP Employee
NXP Employee

Hello,

i.MX6 contains single MIPI CSI to IPU Gasket (CSI2IPU), so one camera can be connected

to it, but  MIPI CSI 2supports up to four concurrent (virtual) channels

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

793 Views
kenyung
Contributor I

But there is only one clk lane, how can we seperate one clk lane to two? is there a ic to seperate the clk lane to two ?

0 Kudos
Reply