How long should I wait for the linux-imx-5.15.5 do_fetch step?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How long should I wait for the linux-imx-5.15.5 do_fetch step?

1,713 Views
yeongungson
Contributor I

yocto_build.pngI purchased imx6q board, and I am building development environment for the first time.

Also, I have no experience with Linux applications.

If you look at the attached image, it only increases the time, and there is no error. Should I just wait?

What should I do in this case?

 

Can anyone give me as much detail as possible?

Labels (1)
0 Kudos
Reply
1 Reply

1,668 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @yeongungson 

Based on the screenshot, which shows tasks for do_fetch broken. Mostly it's caused by network slowness. I would recommend you to start over image build. 

If you still have this problem after re-running. Please share your build platform and the full steps you have taken for this building. 

 

Best regards

Harvey

 

0 Kudos
Reply