How install an Image with new driver on Imx53? thanks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How install an Image with new driver on Imx53? thanks

1,978 次查看
enaud
Contributor III

Hi,

on my pc with windows XP i've installed VMware for configure my kernel with a driver that is missing on SD image.

In VMWAre i've opened the file on DVD Ubuntu.vmx.

Now i view Ubuntu and i've installed LTIB with this command

cd /home/lucid/Desktop/L2.6.35_11.09.01_ER_source

./install


i've lunched LTIB whit this command:

./ltib -c

Now how can install new image on SD with the driver for Sierra SL8092? thanks!

标签 (1)
标记 (2)
0 项奖励
回复
6 回复数

1,874 次查看
enaud
Contributor III

i not have rpm directory on ltib

i must create kernel i think..

but in menu what i must select:

-->platform type imx5x

--> what use packages? Minimum, Test and development, all supported, FSL gnome release package mfg firmware profile?

0 项奖励
回复

1,874 次查看
KrishnaPavan
Contributor II

I have linux source code @ /ltib/rpm/BUILD/ directory.

0 项奖励
回复

1,874 次查看
enaud
Contributor III

i've on Desktop L2.6.35_11.09.01_ER_source Directory

with directory:

pkgs

and files:

EULA

install

ltib.tar.gz

package_manifest.txt

redboot_201003.zip

tftp.zip

0 项奖励
回复

1,874 次查看
KrishnaPavan
Contributor II

Do you have Linux Source Code in the LTIB Directory?

0 项奖励
回复

1,874 次查看
enaud
Contributor III

i not undstand nothing in that discussion!

now i have LTIB on VMware

but i dont know what i must setting in LTIB menù.

0 项奖励
回复

1,874 次查看
KrishnaPavan
Contributor II

Hi enaud,

I think you have already got a solution to this from Donald R Poole Jr  here

http://imxcommunity.org/group/imx53quickstartboard/forum/topics/sierra-sl8092-modem-driver-is-not-pr...

Have you tried this?

Regards :: Krishna Pavan

0 项奖励
回复