Hello Community,
Now i have been working on i.MX 6Solo/ 6 DualLite Applications Processors. Can you please help me how we will briup up the board and what software tools i should install. Please provide me building steps.
Thanks & Regards,
M.Venu Gopal,
7829885192.
what board and OS do you use? you can download the documents from nxp official website as below:
SABRE|Automotive-Infotainment|i.MX6 | NXP
for example ,you use linux, you can download L4.14.78_1.0.0_LINUX_DOCS which is the latest version, then find the document named "i.MX Yocto Project User's Guide" which tell you how to build the image, if you want to use demo image, then pls download "L4.14.78_1.0.0_MX6QDLSOLOX" from the link as below:
SABRE|Automotive-Infotainment|i.MX6 | NXP
for how to program the demo image to the board, pls refer to the "i.MX Linux® User's Guide" from the "L4.14.78_1.0.0_LINUX_DOCS"
Thank you for your response.From: joanxie <admin@community.nxp.com>Sent: Mon, 18 Mar 2019 10:17:48 To: Venu Gopal <venu.gopal@mantratec.com>Subject: Re: - How i will brinup up the i.MX Solo/6DualLite Applications Processors board
NXP Community
Re: How i will brinup up the i.MX Solo/6DualLite Applications Processors board
reply from Joan Xie in i.MX Processors - View the full discussion
what board and OS do you use? you can download the documents from nxp official website as below:SABRE|Automotive-Infotainment|i.MX6 | NXP for example ,you use linux, you can download L4.14.78_1.0.0_LINUX_DOCS which is the latest version, then find the document named "i.MX Yocto Project User's Guide" which tell you how to build the image, if you want to use demo image, then pls download "L4.14.78_1.0.0_MX6QDLSOLOX" from the link as below:SABRE|Automotive-Infotainment|i.MX6 | NXP for how to program the demo image to the board, pls refer to the "i.MX Linux® User's Guide" from the "L4.14.78_1.0.0_LINUX_DOCS"
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in i.MX Processors by email or at NXP Community
Following Re: How i will brinup up the i.MX Solo/6DualLite Applications Processors board in these streams:
Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences
s
This email and any files transmitted with it are confidential and intended solely for the use of the individual or entity to whom they are addressed. If you are not the named addressee you should not disseminate, distribute or copy this e-mail. Please notify the sender immediately by e-mail if you have received this e-mail by mistake and delete this e-mail from your system.Â