How fastest 1000M ethernet speed did imx6q acutally have?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How fastest 1000M ethernet speed did imx6q acutally have?

1,039件の閲覧回数
wyb0116
Contributor II

I made a testing about 1000M ethernet maximum speed on toradex imx6q evaluation board. The board use KSZ8031 phy chip. Did anyone know faster ethernet speed on imx6q chip.

IMG_5863.JPG

ラベル(1)
0 件の賞賛
返信
1 返信

920件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   From erratum ERR004512 (ENET: 1 Gb Ethernet MAC (ENET) system limitation) :


"Limitation of ENET throughput to around 400 Mbps. ENET remains fully compatible to
1Gb standard in terms of protocol and physical signaling. If the TX and RX peak data rate is higher
than 400 Mbps, there is a risk of ENET RX FIFO overrun".

http://www.nxp.com/assets/documents/data/en/errata/IMX6DQCE.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you

0 件の賞賛
返信