How enable LCD8000-43T touch screen with i.MX7 M6.0.1_2.1.0 image?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How enable LCD8000-43T touch screen with i.MX7 M6.0.1_2.1.0 image?

ソリューションへジャンプ
2,119件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX7 SABRE.
I programmed android_M6.0.1_2.1.0_image_7dsabresd image to SD card with MFG tool, and booted it.
However, touch panel on LCD8000-43T was not work even though image was displayed on screen.
Would you let me know how enable LCD8000-43T touch screen?


Best Regards,
Satoshi Shimoda

ラベル(4)
0 件の賞賛
返信
1 解決策
1,388件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

What version of the board do you have? Rev C and later have jumpers J36-J39 that need to be shorted in order for the touch to work.

 

Additionally, you could double check if the DTB file that you are using really enables the touch (it is just required changing the DTB, not rebuilding the complete image).

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,388件の閲覧回数
mike_susen
NXP Employee
NXP Employee

Hi Satoshi,

Short pins 1-2 on jumper JP1 on sabre board.

Michal

0 件の賞賛
返信
1,388件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Mike,

Thank you for your reply,

But JP1 1-2 pins have been shorted as the attached image.

IMG_0296.JPG

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,388件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

Have you selected the proper DTB file to enable the LCD screen? Or is your problem that just the touch is not working but the screen is properly displaying the image?

Best regards!

/Carlos

0 件の賞賛
返信
1,388件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Carlos,

I'm using android_M6.0.1_2.1.0_image_7dsabresd image without any change, so DTB file is not changed from default.

> Or is your problem that just the touch is not working but the screen is properly displaying the image?

Yes, my problem is just the touch since image is displayed properly.

The touch is not enabled by android_M6.0.1_2.1.0_image_7dsabresd?

In the case, I have to build a image which enables the touch.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,389件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Satoshi,

What version of the board do you have? Rev C and later have jumpers J36-J39 that need to be shorted in order for the touch to work.

 

Additionally, you could double check if the DTB file that you are using really enables the touch (it is just required changing the DTB, not rebuilding the complete image).

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信