How do we use iMX8QM's uart to recieve GNSS module data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do we use iMX8QM's uart to recieve GNSS module data

2,211 次查看
Tamako
Contributor I

Now  I have an iMX8QM ,I want to use it to recieve GNSS module ,but I can't test the uart of iMX8QM ,beacuse it looks like the iMX8QM just only have 5 uarts ,LP1 and LP2 is using to debug the core of A72 and A53,and another 1 is using to bluetooth module ,the last of 2 is connecting to the 2 M4 cores,I want to konw how I use the GNSS module connect to uart to revieve data?

0 项奖励
回复
6 回复数

2,186 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can choose one uart if you don't use it for other function, to enable it in the dts file you use

0 项奖励
回复

2,181 次查看
EmptyObject_
Contributor I

 I can not use lpuart3/lpuart4,how do i use this two lpuart ?For me ,l just can use this two lpuart ,and I have enabled the two  in the dtb file,but I can not use.

0 项奖励
回复

2,149 次查看
joanxie
NXP TechSupport
NXP TechSupport

besides this, pls don't forget add this

--- a/arch/arm64/boot/dts/freescale/imx8qm-ss-dma.dtsi
+++ b/arch/arm64/boot/dts/freescale/imx8qm-ss-dma.dtsi
@@ -146,6 +146,8 @@

&lpuart3 {
compatible = "fsl,imx8qm-lpuart", "fsl,imx8qxp-lpuart";
+ dmas = <&edma2 13 0 0>,
+ <&edma2 12 0 1>;
};
0 项奖励
回复

2,145 次查看
EmptyObject_
Contributor I
I got a new question about lpuart now ,I did the loopback test,I send a string once ,but the rx

recieved three times ,and I checked all the lpuart ,there are all the same situation.Do you know how to resolve it?
0 项奖励
回复

2,132 次查看
joanxie
NXP TechSupport
NXP TechSupport

I already found you created a new case for this issue, pls follow that case for the new issue

0 项奖励
回复

2,155 次查看
joanxie
NXP TechSupport
NXP TechSupport

I don't know what bsp you use, as I mentioned before, pls check the dts file you use, then enable it in the dts, for example

https://github.com/nxp-imx/linux-imx/blob/lf-5.15.y/arch/arm64/boot/dts/freescale/imx8qm-mek.dts

you can find lpuart3 is disabled, you need set it to OK if you need to use it, this is just for reference, you can set by yourself on your own bsp

0 项奖励
回复