How do i build a 5.1 surround sound system with i.mx6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do i build a 5.1 surround sound system with i.mx6?

1,176件の閲覧回数
hi_shawn
Contributor II

Hi FSL guys,

Good day.

One of my customers  will set a project which is used to play 5.1 surround sound only. For ESAI and IIS, i'm not quiet sure which one is more approval. Could you please tell me the better choice ? Any other suggestions will be welcome.  Thanks. 

ラベル(1)
0 件の賞賛
返信
1 返信

1,093件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Shawn

seems esai is preferable option, please check for available codecs in

sect.28.2 SoC Sound Card attached Linux Manual. CS42888 esai codec used

on i.MX6 Sabre AI boards.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信