Hello,
I am posting this because I couldn't figure out from the existing solutions.
I have imx6dl based custom board with GPS antenna connected to UART2.
Once in a while I see the error 'imx-uart 21e8000.serial: Rx FIFO overrun'.
The same issue is posted here: iMX6Quad uart RX Fifo Overrun and also in many threads.
The answers I got are like to implement hardware flow control OR increase the CPU frequency to maximum.
If I implement the hardware flow control, as per a thread here UART errors: "Rx FIFO overrun" and "overwrite!"
when the RX FIFO is full already I wont be receiving the data. (Is this correct? If so I will lose GPS data).
I also increased the CPU Frequency to Maximum:
root@US16SIQC:~# cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_max_freq
792000
root@US16SIQC:~# cat /sys/devices/system/cpu/cpu1/cpufreq/cpuinfo_cur_freq
792000
root@US16SIQC:~# cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
performance
But I still see the problem.
One more observation is that CPU0 is only loaded and CPU1 seems to be free:
root@US16SIQC:~# cat /proc/interrupts
CPU0 CPU1
29: 295735 95769 GIC 29 twd
34: 0 0 GIC 34 sdma
51: 0 0 GIC 51 rtc alarm
54: 89359 0 GIC 54 mmc0
55: 1438 0 GIC 55 mmc1
56: 11376 0 GIC 56 mmc2
57: 94462 0 GIC 57 mmc3
59: 156342579 0 GIC 59 21e8000.serial
61: 8530 0 GIC 61 21f0000.serial
64: 0 0 GIC 64 200c000.ecspi
65: 0 0 GIC 65 2010000.ecspi
69: 83 0 GIC 69 21a4000.i2c
70: 100 0 GIC 70 21a8000.i2c
72: 68 0 GIC 72 2184200.usb
75: 0 0 GIC 75 2184000.usb
79: 0 0 GIC 79 202c000.ssi
81: 0 0 GIC 81 imx_thermal
87: 0 0 GIC 87 i.MX Timer Tick
150: 79751 0 GIC 150 2188000.ethernet
151: 0 0 GIC 151 2188000.ethernet
256: 0 0 gpio-mxc 0 2194000.usdhc cd
IPI0: 0 0 CPU wakeup interrupts
IPI1: 0 0 Timer broadcast interrupts
IPI2: 83871 193191 Rescheduling interrupts
IPI3: 0 0 Function call interrupts
IPI4: 6502 5527 Single function call interrupts
IPI5: 0 0 CPU stop interrupts
IPI6: 0 0 IRQ work interrupts
IPI7: 0 0 completion interrupts
Err: 0
Here, CPU1 is not being used much. Can I dedicate this CPU to only work on the UART2? Is this possible? How Can I balance the load between CPUs? If I can achieve this is there a possibility to fix the issue?
I am using linux kernel: 3.18.29 with openWRT Chaos Calmer.
Thanks,
Ramana
Hi Ramana
to dedicate some CPU to module interrupt one can look at irq affinity discussion
https://community.freescale.com/thread/301130
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I have increased the frequency and also tied the interrupt to CPU1. Now the FIFO overrun print is seen very rarely. What would be your suggestion to aviod this completely? Also what is the best way to reproduce this error?