How do I enter Bootstrap mode on an IMX50EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I enter Bootstrap mode on an IMX50EVK?

654 Views
conorross
Contributor I

What is the dip switch setting for bootstrap mode on the IMX50EVK?

Labels (1)
0 Kudos
1 Reply

520 Views
igorpadykov
NXP Employee
NXP Employee

Hi Conor

for bootstrap mode boot pins should be set as:

BOOT_MODE[1:0] =11  - USB Downloader

and one can look at attached EVK schematic p.10

for S1 dip-switch postions.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos