How do I configure mmc0 to 208MHz on MCIMX6ULL-EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I configure mmc0 to 208MHz on MCIMX6ULL-EVK?

744 Views
JohnKlug
Senior Contributor I

I am seeing:

 

root@imx6ullevk:~# cat /sys/kernel/debug/mmc0/ios 
clock:          132000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      2 (4 bits)
timing spec:    6 (sd uhs SDR104)
signal voltage: 1 (1.80 V)
driver type:    0 (driver type B)


How do I get the interface to use the 200MHz clock?   What should I put in device tree?

0 Kudos
Reply
3 Replies

705 Views
JohnKlug
Senior Contributor I

I mean the large SD card port on the EK board, which is capable of 1.8 or 3.3V.

This is what I did to create my repo:

repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml

I did not change the kernel or device tree.

0 Kudos
Reply

709 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do you mean emmc or sd card here? Which version BSP are you using?

0 Kudos
Reply

693 Views
JohnKlug
Senior Contributor I

The 132000000 is found in device tree here:
usdhc assigned-clock-rates 

This found in change:
SDIO CLOCK CHANGE 

 

Apparently due to a chip errata:

MLK-13188-2 dts: imx6ull: change the usdhc root clock to 396MHz
Due to the errata ERR010450 limit, this patch change the imx6ull
usdhc root clock to 132MHz in soc related dts file, remove all
the root clock setting in board dts file, after this patch,
SDR104/HS200 work at 132MHz, DDR50/DDR52 work at 33MHz.
0 Kudos
Reply