Hi,
How do I compile an appropriate image for xen without EVS in android AUTO 9.0?
android_p9.0.0_1.0.2-auto-beta_image_8qmek2.tar.gz
The android demo released contains the image available for xen, but it is aimed at EVS function, but it cannot be displayed properly on my board (imx8qm mek). I think it is because EVS function needs M4 core to work together, because my board is A0 version, and M4 core is not used to start the system.The image without EVS can start normally, but there is no xen adaption, so I would like to ask: is there any way to directly compile the image without EVS function but also ADAPTS xen?