Igor,
The patch says that it is for the JB4.2.2-1 BSP, and we are using KK4.4.2 BSP. Is this a problem for the patcher, or were there no major changes between the two releases? Furthermore, when we built our work environment, we did apply a patch (as instructed by Freescale). I am not sure if this patch accomplished the same changes that you recommend. From the "How-To" manual:
"
.../uboot-imx$ cd /android/WorkArea/
.../WorkArea/$ source /android/android_kk4.4.2_1.0.0-ga_core_source/code/kk4.4.2_1.0.0-ga/and_patch.sh
.../WorkArea/$ help //"c_patch" function should be visible
.../WorkArea/$ c_patch /android/android_kk4.4.2_1.0.0-ga_core_source/code/kk4.4.2_1.0.0-ga imx_kk4.4.2_1.0.0-ga
Should see SUCCESS: Now you can build the Android code for FSL i.MX platform
"
-Michael
Edit: This seems to indicate to me that we have already applied the patch. Is there another solution we can try?