Hi All,
I am working on an Android project that is base on the SabreSD reference design. I am having problems finding the procedure for permanently setting the MAC address on eth0. I need to be able to give each unit a unique MAC address. Thanks.
解決済! 解決策の投稿を見る。
OK, so putting it all together after calculating the requisite indices and deciphering table 5-10 in the reference manual:
If I want to program MAC address 10:98:76:54:32:10 into my i.mx6 Android device I enter the following uboot commands:
imxotp blow --force 23 1098
imxotp blow --force 22 76543210
boot the unit and enter the following command in the debug console:
busybox ifconfig
verify that the HWaddr for eth0 matches the desired MAC address. In this example:
# busybox ifconfig
eth0 Link encap:Ethernet HWaddr 10:98:76:54:32:10
inet addr:192.168.2.93 Bcast:192.168.2.255 Mask:255.255.255.0
inet6 addr: fe80::210:25ff:fe0a:fb9a/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:161 errors:0 dropped:36 overruns:0 frame:0
TX packets:11 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:15836 (15.4 KiB) TX bytes:1377 (1.3 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
I have tried the above on our board and it worked.
Thanks,
Jim Pieterick
Can some one please help with below q's
Q1 . How to get imxopt tool and is this tool helps me to make "fixed" the MAC address for below registers
In i.MX 6Solo/6DualLite application processors
21B_C620 (Absolute address) -Value of OTP Bank4 Word2 (MAC Address) (OCOTP_MAC0)
21B_C630(Absolute address) - Value of OTP Bank4 Word3 (MAC Address) (OCOTP_MAC1)
Q2. I found two types of MAC's : HW_OCOTP_MAC0/MAC1 which is in /sys/fsl_otp/HW_OCOTP_MAC0/MAC1
above registers are same as Value of OTP Bank4 Word2/3 (MAC Address) (OCOTP_MAC0/1) ??
if both are same then,then below flashing procedure is correct or not for permanently fixing the MAC address
Say for eg the MAC address to be set is 00:23:a1:47:1b:80
echo 0x00000023 >/sys/fsl_otp/HW_OCOTP_MAC1
echo 0xa1471b80 >/sys/fsl_otp/HW_OCOTP_MAC0
-Thanks,
kalyan.
Hi James
mac address is stored in fuses, description can be found in
Table 5-10. Fusemap Descriptions i.MX6DQ Reference Manual (rev.2 7/2014)
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
Q&A: How to program i.MX6 eFUSE?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
From "Q&A How to program i.MX6 eFUSE"
--------------------------------
U-Boot contains a tool, imxotp, which is used for fusing.
U-Boot > imxotp
imxotp - One-Time Programable sub-system
Usage:
imxotp imxotp read <index>
- read fuse at 'index'
imxotp blow [--force] <index> <value>
- blow fuse at 'index' with hex value 'value'
Tips: 'addr' to 'index':
convert 'index' from 'address'
index = (addr - otp_base) / 0x10
eg, addr is 0x021bc410, otp_base is 0x021bc400, the index = 1
--------------------------------
I don't understand how to calculate the index. Table 5.10 indicates that the fuse address for the MAC_ADDR[31-0] fuse is "0x620[31:0]" and the address for MAC_ADDR[32:47] is 0x630[15:0]. If I subtract otp_base (0x021bc400) from one of these addresses as the index equation above indicates, I will get a negative number. It looks like the fuse address needs to be added to some offset to get the value needed for the addr parameter in the index equation. What is that offset? otp_base?
Thanks,
Jim Pieterick
Hi James
when Table 5.10 indicates that the fuse address for the MAC_ADDR[31-0] fuse is "0x620[31:0]"
this means addr is 0x021bc620
Best regards
igor
OK, so putting it all together after calculating the requisite indices and deciphering table 5-10 in the reference manual:
If I want to program MAC address 10:98:76:54:32:10 into my i.mx6 Android device I enter the following uboot commands:
imxotp blow --force 23 1098
imxotp blow --force 22 76543210
boot the unit and enter the following command in the debug console:
busybox ifconfig
verify that the HWaddr for eth0 matches the desired MAC address. In this example:
# busybox ifconfig
eth0 Link encap:Ethernet HWaddr 10:98:76:54:32:10
inet addr:192.168.2.93 Bcast:192.168.2.255 Mask:255.255.255.0
inet6 addr: fe80::210:25ff:fe0a:fb9a/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:161 errors:0 dropped:36 overruns:0 frame:0
TX packets:11 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:15836 (15.4 KiB) TX bytes:1377 (1.3 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
I have tried the above on our board and it worked.
Thanks,
Jim Pieterick