I am trying to build a kernel (3.0.35) with PREEMPT_RT patch for my imx6q-sdb. (sabre sdb)
I use BSP "L3.0.35_4.0.0_130424_source".
I am capable of doing the following:
Build the kernel with applied patches supplied by the bsp.
Patch the kernel supplied (3.0.35) with the preempt_rt patch. (rtKernel)
I am doing all the patching manually at this point... as I was unable to find information on how to "offcially" apply a patch to the kernel in the configuration phase of ltib
When I try to patch the bsp patches over my rtKernel both the git script and "patch" fail.
Did someone already get all the bsp patches applied (with preempt_rt)?
Is there a different set of patched that would work together with the preempt_rt patch?
As I have not found any information on this could you please point me into the right direction if there is?
Thanks in advance for any help you can give.
 
					
				
		
 fabio_estevam
		
			fabio_estevam
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Try using 3.10.9 and then you can patch it directly with the latest rt patches:
I have no problem applying the rt patch to the 3.0.35 kernel. My problem is applying both, the bsp patches (which only add support and drivers for the board) AND the rt-patch.
Or are you implying that the 3.10.09 kernel already has all the drivers, freescale software etc. needed for the imx6q sabre-sd board to fully function?
 
					
				
		
Peter
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
 
					
				
		
Peter
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel
free to reply with an update to this discussion.
Thanks,
Yixing