How display AVI video stream imx.6 (Linux 3.10.17) to PC (Ubuntu 3.13.0-44)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How display AVI video stream imx.6 (Linux 3.10.17) to PC (Ubuntu 3.13.0-44)

2,257 Views
reinholdfrederi
Contributor I

Hi,

I would like to display a stream AVI video file from i.mx6 to PC based on Ubuntu with g-streamer 0.10 with plugin 'base' and 'good'.

I have tried with this parameters:

  • Server: iMX6
CLIENT_IP=10.251.101.58  
FILE=Video_1080p.avi  
gst-launch filesrc location=$FILE   typefind=true ! aiurdemux  ! queue  ! rtpmp4vpay ! udpsink host=$CLIENT_IP -v 

Console:

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/mpeg, mpegversion=(int)4, parsed=(boolean)true, width=(int)1920, height=(int)1080, framerate=(fraction)5000000/208333

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = video/mpeg, mpegversion=(int)4, parsed=(boolean)true, width=(int)1920, height=(int)1080, framerate=(fraction)5000000/208333

/GstPipeline:pipeline0/GstRtpMP4VPay:rtpmp4vpay0.GstPad:sink: caps = video/mpeg, mpegversion=(int)4, parsed=(boolean)true, width=(int)1920, height=(int)1080, framerate=(fraction)5000000/208333

/GstPipeline:pipeline0/GstRtpMP4VPay:rtpmp4vpay0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)1, config=(string)000001b001000001b58913000001000000012000c48d8800c53c04871463000001b24c61766335312e34342e30, payload=(int)96, ssrc=(uint)1834147004, clock-base=(uint)462164955, seqnum-base=(uint)16877

/GstPipeline:pipeline0/GstRtpMP4VPay:rtpmp4vpay0: timestamp = 462164955

/GstPipeline:pipeline0/GstRtpMP4VPay:rtpmp4vpay0: seqnum = 16877

/GstPipeline:pipeline0/GstUDPSink:udpsink0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)MP4V-ES, profile-level-id=(string)1, config=(string)000001b001000001b58913000001000000012000c48d8800c53c04871463000001b24c61766335312e34342e30, payload=(int)96, ssrc=(uint)1834147004, clock-base=(uint)462164955, seqnum-base=(uint)16877

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

  • Client: Ubuntu PC

CAPS=application/x-rtp,media=(string)video,clock-rate=(int)90000,encoding-name=(string)MP4V-ES,

profile-level-id=(string)1,config=(string)000001b001000001b58913000001000000012000c48d8800c53c04871463000001b24c61766335312e34342e30,

payload=(int)96,ssrc=1303818908,clock-base=1090442294,seqnum-base=(uint)63287

PORT=5000

gst-launch udpsrc port=$PORT ! $CAPS ! rtpmp4vdepay ! queue ! ffdec_mpeg4 ! xvimagesink sync=false -v

Console:

bash: ./ReceiverVideoPC_MP4.sh: ligne 3: Erreur de syntaxe près du symbole inattendu « string »

bash: ./ReceiverVideoPC_MP4.sh: ligne 3: `profile-level-id=(string)1,config=(string)000001b001000001b58913000001000000012000c48d8800c53c04871463000001b24c61766335312e34342e30,'

What's the good parameters ?

Thanks for your response.

Labels (2)
0 Kudos
Reply
3 Replies

1,689 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Frederic,

Please review the following document, it shows how to do the streaming and it was based on VLC

GStreamer RTP Streaming


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,689 Views
reinholdfrederi
Contributor I

Hello jamesbone,

I must only set VIDEO_SRC in sender script: VIDEO_SRC=filesrc location=$FILE ?


Nice day

Frederic

0 Kudos
Reply

1,689 Views
saurabh206
Senior Contributor III

Hi,

Send your post to imx community (e.g. i.MX Community ) to get it visible for active members.

Saurabh

0 Kudos
Reply