How configure a pin as Open Drain for i.MX7D using the config tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How configure a pin as Open Drain for i.MX7D using the config tool

ソリューションへジャンプ
1,842件の閲覧回数
HOTA
Contributor III

Hi,

How can I configure a pin as Open Drain for i.MX7D using the config tool?

I was unable to find the option to configure it.
Also, please tell me how to configure it as an interrupt PIN in the same way.

HOTA_1-1692951375039.png

 

 

I use Ver 13.1.

HOTA_0-1692951335695.png

Thanks,

HOTA

0 件の賞賛
返信
1 解決策
1,768件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @HOTA,

One cannot configure interrupt for a pin from i.MX Config tool.

One has to make changes in the device tree. Please refer to imx7d-sdb.dts, specifically to the tsc2046 node.

Thanks & Regards,
Ritesh M Patel

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,823件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @HOTA,

I hope you are doing well.

i.mx7D pins cannot be configured in Open Drain IO mode.

One can refer to the below-mentioned link for more details:

https://community.nxp.com/t5/i-MX-Processors/i-mx7-GPIO-open-drain-mux/m-p/787035/highlight/true

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信
1,815件の閲覧回数
HOTA
Contributor III

Hi @riteshmpatel ,

Thank you for your answer.
How should I configure the interrupt PIN?
I now understand about open-drain. Thank you!

 

Thanks,

HOTA

0 件の賞賛
返信
1,769件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @HOTA,

One cannot configure interrupt for a pin from i.MX Config tool.

One has to make changes in the device tree. Please refer to imx7d-sdb.dts, specifically to the tsc2046 node.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信
1,757件の閲覧回数
HOTA
Contributor III

hi @riteshmpatel ,

I understand. Thank you.

Thanks,

HOTA

0 件の賞賛
返信