How can i enable usb at imx6 while conect to PC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i enable usb at imx6 while conect to PC

1,477 Views
vyasvenkat1996
Contributor I

As i mount gadgetFS and and connect the imx6 board to PC after command at PC i.e lsusb I am unable to get usb port for the imx6 , what steps i have to follow to enable the usb port for imx6.

As i am using yocto project for kernel customizing.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,417 Views
igorpadykov
NXP Employee
NXP Employee

Hi venkat

one can try to follow sect.10.3.7 USB attached Linux Manual

with Demo Images from link

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply