Hello, I am currently working on a project with the iMX93 EVK board. I am trying to control an interface by running a blinking LED example, but I'm having trouble figuring out how to use the RPi GPIO header.
I suspect that the RPi GPIO header is associated with 'gpiochip2'. I tried using GPIO line 0, assuming it was related, but the LED didn't respond. I also tried changing the line to 17 (the BCM number), but that didn't work either. I ruled out a hardware issue because the LED lights up when I connect it directly to 3.3V.
Could you please guide me on how to resolve this issue? Which documentation should I refer to for more information?
Below is the Python code I executed:
import gpiod
from gpiod.line import Direction, Value
import time
LINE = 17
with gpiod.request_lines(
"/dev/gpiochip2",
consumer="blink-example",
config={
LINE: gpiod.LineSettings(
direction=Direction.OUTPUT, output_value=Value.ACTIVE
)
},
) as request:
while True:
request.set_value(LINE, Value.ACTIVE)
time.sleep(1)
request.set_value(LINE, Value.INACTIVE)
time.sleep(1)
解決済! 解決策の投稿を見る。