How can I use IIC module in imx257? Is there a detailed reference manual?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I use IIC module in imx257? Is there a detailed reference manual?

737 Views
zhangjun972845
Contributor I

for example,How do I operate the register, when and other IIC module when communicating?

Labels (1)
0 Kudos
2 Replies

538 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

for i2c usage one can look at attached i.MX25 Linux Manual

Chapter 20 Inter-IC (I2C) Driver and use i2c tools

All Boards I2C-tools

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

538 Views
zhangjun972845
Contributor I


hi ,igorpadykov,  thanks for help ,but  another question, I will use the iic moudle as smbus with a RTC system. when i use the IIC driver for rtc(iic interface ) ,it is good, but the same drive  to battery(SMBUS interface), it can not send  Repeat start, I do not know why. so I may need you help. can you give me some PDF,or code to operate the IIC moudle ?

0 Kudos